May 2009

 

Siemens enhances functionality of Simatic Maintenance Station


Siemens has upgraded the Simatic Maintenance Station software for the diagnosis and maintenance of plants and machinery, with new features focusing on diagnostic functionality and plant asset management.

 

Simatic Maintenance Station, a software option for the Simatic WinCC SCADA system, supports preventive, condition-based and reactive maintenance activities of a plant in a central system. It
now offers functions for the efficient planning and monitoring of maintenance operations and jobs. It also allows devices in the field to access the Simatic Maintenance Station via a web client for remote maintenance, for example, panel PCs with touch controls can be used to carry out diagnostic measures on-site.

 

The software visualises diagnostic and maintenance information – from a PC to network components, all the way to controllers, switching, protection and control units, as well as drives. The plant operator receives a uniform and clear status display. Using this, they can clearly identify components, systems and plant units, assess them individually, and, where appropriate, respond quickly to special situations. Based on the condition of the components, appropriate measures for machinery and plant maintenance can be undertaken at the right time to reduce or even avoid downtimes. This contributes directly to lower maintenance costs and higher productivity.

 

Simatic Maintenance Station passes on maintenance requests to other target systems, for example, a computer. All operations are message-based and are therefore easy to archive and understand. This results in an extensive database that can be analysed with WinCC.

 

The configuration of Maintenance Station is easy, because it uses Step 7 project data that is already available from the plant set-up phase. Components from other manufacturers are incorporated using standards-based procedures.

 

Siemens. Innovation for generations.

 

For more information, please contact Siemens in Australia and in New Zealand using the contacts box below.

Siemens Reference Number: P-I-2009-26 

Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com
|

Solution Areas

Solutions - Go

Related Links

About Siemens Australia & New Zealand