Siemens is complementing its Simatic Human Machine Interface (HMI) device series with all-round IP65 protection with modular expansion units. The new components in the design of the HMI devices are individually equipped for plant-specific operator control and monitoring tasks, for example, with illuminated pushbuttons, lamps, switches, USB ports or emergency stop buttons.
The expansion units are suitable for all Simatic HMI devices with all-round IP65 protection and are optionally attached on the left side, right side, or both sides of the Multi Panel 377 Pro 15”, Thin Client Pro 15”, or Flat Panel Monitor Pro 15”.
The complete system comprising an HMI device and expansion units achieve degree of protection IP65 and now permits additional control activities and applications directly on-site at the operator station.
The expansion units are also wired up directly to the support arm system, independently of the HMI device, so that the wiring does not have to be disconnected for maintenance or replacement of the HMI device.
Siemens. Innovation for generations.
For more information, please contact Siemens using the contacts box below.
Photograph caption:
Siemens is complementing its Simatic HMI device series with all-round IP65 protection with modular expansion units. The new components in the design of the HMI devices are individually equipped for plant-specific operator control and monitoring tasks, for example, with illuminated pushbuttons, lamps, switches, USB ports or emergency stop buttons.