April 2009

 

Siemens safety device saving lives


Siemens LDS6 laser gas analyser is helping to improve safety and save millions of dollars in damage repairs for Tasmanian Electro Metallurgical Company (TEMCO), a subsidiary of BHP Billiton, by alerting its manganese ferroalloy plant workers to an imminent furnace explosion in time to prevent it.

 

Mr. Paul Dennis, Process Technology Supervisor at TEMCO, explained the common cause of explosions in the submerged arc furnaces, which are identified as the most dangerous furnaces in the world.

 

“Sudden explosions are known to arise in these furnaces due to the temperature control mechanism, which pumps water through a series of tubes inside the furnace to maintain the internal temperature.  Over time, the water eventually erodes these steel tubes and this allows some water to leak into the furnace,” Mr. Dennis said.

 

“The extremely high furnace temperatures and increasing water leakage are the main causes of the sudden explosions. At 400°C to 600°C, the water that enters the furnace through the eroded steel tubes is immediately converted into steam.  As this erosion continues and causes more steam to accumulate inside the furnace, the internal pressure builds up until it eventually explodes.”

 

Mr. Brendan Welsh, Siemens Product Manager, explained the technology behind the LDS6 laser gas analyser and challenges Siemens had to overcome for this application.

 

“As this was a first time application for the LDS6 in submerged arc furnaces on a global scale, great caution had to be taken in order to guarantee its accuracy, sensitivity, reproducibility, reliability and maintainability,” Mr. Welsh said.

 

“One of the major challenges was to counteract the extremely high levels of dust present at the facility.  Around 100 grams of dust per cubic metre was recorded, which ordinarily, was much too high for the laser analyser to work accurately.

 

“Siemens modified the analyser specifically to address this challenge. Extensive consultation occurred between Siemens manufacturers in Germany, a Siemens authorised reseller and BHP Billiton to develop an analyser which was suitable. We built an air chamber that’s used to blow the dust off the laser every few minutes. This allows the laser to gain an accurate scan of the water levels and consequently, delivers consistent and reliable readings.

 

“Trials undertaken by Paul Dennis enabled a set of control limits to be established, with the analyser detecting water leaks several hours before any other traditional methods have been able to. These limits are used to foreworn of any future explosions, so that plant workers can take the appropriate safety measures, including shutting down the facility if needed.”

 

Mr. Dennis said the safety procedure developed around the Siemens analyser was a significant step towards achieving zero fatalities in the highly volatile and unpredictable environment around plant furnaces.

 

”I’m hopeful that with the new LDS6 analyser, submerged arc furnaces will not be the cause of any safety issues for BHP Billiton. Safety issues are of critical concern for TEMCO and BHP Billiton, and we are considering other applications of the LDS6 within our operations and the operations of other industries, such as mining, around the world,” he said.

 

The only plant of its kind in Australia, TEMCO supplies the critical steel additive manganese ferroalloy to more than 50 companies around the world.  With their four electric arc furnaces, TEMCO can produce more than 250,000 tonnes of manganese alloys per year, 80 percent of which is exported. This can now be achieved more safely than ever with the aid of Siemens LDS6 gas analyser.

 

Mr. Dennis has made a significant contribution towards safety in the minerals process industry. In formally recognising this invaluable contribution, BHP Billiton recently awarded Mr. Dennis with the Excellence in Safety Award. His extensive research into understanding the sporadic nature of submerged arc furnaces, accurately measuring water levels, predicting explosions and establishing safety standards has already enabled critical decisions to be made that have prevented imminent furnace explosions.

 

Siemens. Innovation for generations.

 

For more information, please contact Siemens in Australia and New Zealand using the contacts box below.

Siemens Reference Number: P-I-2009-19 

Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com
|

Solution Areas

Solutions - Go

Related Links

About Siemens Australia & New Zealand