January 2009

 

Flow instruments equipped with Foundation Fieldbus interface


Siemens has developed a new communication module for connecting flow instruments to the Foundation Fieldbus (FF). The module is suitable for the series of Sitrans F M 6000 and Sitrans F C MASS 6000 devices, which are part of the USM II (Universal Signal Module) family.

 

Based on the "plug-and-play" principle, the user simply clicks the module into the mount of the instrument. And depending on the desired communication method, next to the new FF module there are additional communication modules available such as for Profibus PA/DP, Hart, Modbus RTU and DeviceNet.

 

Siemens. Innovation for generations.

For more information, please contact Siemens using the contacts box below.

 

Photograph caption:

Siemens has developed a new communication module for connecting flow instruments to the Foundation Fieldbus (FF). The module is suitable for the series of Sitrans F M 6000 and Sitrans F C MASS 6000 devices, which are part of the USM II (Universal Signal Module) family.

Siemens Reference Number: P-I-2009-02 

Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com
|

Solution Areas

Solutions - Go

Related Links

About Siemens Australia & New Zealand