March 2008

 

High-availability, safe and fault-tolerant controller


A new controller for high-availability, safe and fault-tolerant applications in the process industry has been developed by Siemens. The Simatic CPU S7-412-3H complements the range of products of the Simatic-S7-400H family of controllers in the lower performance range. The new device is suitable for applications involving high-availability functions for monitoring and closed-loop control of temperatures, liquid levels and emergency power generators as well as safe, fault-tolerant solutions with maximum safety integrity levels up to SIL 3, for example for burners.

 

Safety functions can be added with the S7 F Systems software package. The safety functions are parameterized by the user in CFCs (Continuous Function Charts) by means of function blocks provided or using cause & effect methods in the Simatic Safety Matrix, the safety lifecycle tool. As with all controllers of the S7-400H family, standard and safety functions can be combined in the controller and on the I/O level in the case of the S7-412H as well.

 

For more information or enquiries relating to this media release, please use the contacts box below.

Siemens Reference Number:  

Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com
|

Solution Areas

Solutions - Go

Related Links

About Siemens Australia & New Zealand