Home
Contact Siemens
Sitemap

SIMATIC Maintenance Station

August 2007

 

SIMATIC Maintenance Station is now available

The SIMATIC Maintenance Station 2007 is a NEW software option for diagnostics and plant-related asset management on the basis of STEP 7 and WinCC.

 

  • Option package for STEP7 V5.4 and WinCC V6.2 for diagnostics and maintenance of machines and plant
  • Generation of a WinCC maintenance view for a STEP 7 project / multi-project

 

Features

With Totally Integrated Automation, the same system can be used for automation and maintenance: SIMATIC WinCC, the SCADA system for Totally Integrated Automation.

The resulting information is selectively divided to prevent the operators and maintenance engineers from being flooded with information.

To achieve this, a maintenance station is introduced in addition to the actual SCADA system. The operator can use the SCADA station to access all of the process-relevant information and can manually intervene in the plant sequence. Maintenance-relevant information is kept away from the SCADA station. This information is presented for the maintenance engineer on the maintenance station.

It is irrelevant whether the SCADA system and the maintenance station are executed on a common computer or on separate computers. Since the same HMI tools are used, switching over of the display between the SCADA system and the maintenance station is possible at any time.

SIMATIC Maintenance Station features:

 

  • Automatic generation of a maintenance view in WinCC, derived from the STEP 7 hardware configuration
  • I&M Online data are allowed for in the I&M group export
  • Visualization of all automation components for the whole plant, from management to field level, in ready linked hierarchically arranged WinCC images

 

Representation of central and distributed SIMATIC S7 components, PROFIBUS and PROFINET networks and associated bus nodes

Ethernet network components and industry PCs can be connected via the SIMATIC Net SNMP OPC Server

 

  • Display of the device statuses with group status generation in overview and detail images
  • Support of the device conditions “Maintenance requirement“ and “Maintenance request“ for condition-based maintenance
  • Provision of uniform faceplates for the display of detail information for all depicted components
  • Display of device identification data (electronic type label)
  • Forwarding of maintenance requests directly from WinCC
  • Integrated display of the request status


Benefits

An automation system incorporating the SIMATIC Maintenance Station provides:

 

  • Reduction of standstill times:
    Problems in the plant are identified more quickly due to the uniform and clear representation of information that is maintenance relevant
  • Prevention of standstill times:
    Support of condition-based maintenance
  • Reduction of maintenance costs:
    Optimization of the information flow between production and maintenance by forwarding maintenance requests and display of the request status
  • Transparency and traceability:
    All events are message-based and can thus be archived and traced
    An extensive database is created that can be analyzed with WinCC means or other external tools
  • Scalability:
    Support of WinCC single-user stations and Client Server configurations.
    The SIMATIC Maintenance Station can be added to an existing WinCC project
  • Consistency:
    The maintenance view is generated from the control project and is consistent with the latter
  • Flexibility in the choice of devices:
    Use of PROFIBUS and PROFINET standards for device integration
    Additional proxy concept permits depiction of devices that are not part of the STEP 7 Hardware Configuration or that do not support the standard diagnostics of PROFIBUS / PROFINET

  

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Licensing

The SIMATIC Maintenance Station comes as a basic package containing all the tools required for configuration of a Maintenance Station, as well as a Runtime License for the display of 100 devices. Power Packs for 100, 500 or 1000 devices are available for the operation of installations with larger quantity frameworks. They are simply added and can be combined at random.

The preconditions for the configuration of the SIMATIC Maintenance Station are a STEP 7 license (V5.4 and higher), a WinCC RC license (V6.2) and, if necessary, the SIMATIC Net licenses for the plant configuration.

 

The preconditions for the operation of a SIMATIC Maintenance Station are the WinCC licenses (V6.2) as required for the plant configuration.

Countable devices are:

 

  • AS systems
  • Distributed devices (PROFIBUS / PROFINET)
  • PCs
  • Network components
  • Asset Proxies

 

The SIMATIC Maintenance Station supports German / English / French / Italian / Spanish. The messages displayed by the Maintenance Station can be translated in STEP 7 by the user into other languages as well.

 

Device Preconditions for Integration
Type Integration Remark
SIMATIC S7 controllers / I/Os
S7-300 * Yes
S7-400 Yes
Win AC Yes
Distributed devices
ET200 Yes PROFIBUS-DP and PROFINET IO acc. to STEP 7 Hardware Catalog
PROFIBUS standard slaves Yes integration via GSD file
PROFINET standard devices Yes integration via GSD filetei
Network components
Ethernet network components Yes SIMATIC Net SNMP OPC Server and MIB required in addition
PROFINET network components Yes
PROFIBUS diagnostic repeater Yes
Personal Computers
PCs / Industry PCs Yes SIMATIC Net SNMP OPC Server required in addition
Drives
Drives with PROFIBUS connection Yes Devices acc. to PROFIDRIVE profile require Drive ES SIMATIC (V5.4 SP1 and higher) for integration
Drives with PROFINET connection Yes Devices acc. to PROFIDRIVE profile require Drive ES SIMATIC (V5.4 SP1 and higher) for integration
Other devices
Devices not included in STEP 7 Hardware Config Yes Integration via fuction block (Asset Proxy)

* In the case of S7-300 PLCs only PROFIBUS / PROFINET systems connected to the internal CPU interfaces are supported.


Software Requirements
System Operating System
Engineering Station "ES" Windows XP Professional SP2 / Windows Server 2003 SP1
Maintenance Station Stand-alone / WinCC Station "Single-user" Windows XP Professional SP2 / Windows Server 2003 SP1
ES with Maintenance Station Stand-alone Windows XP Professional SP2 / Windows Server 2003 SP1
Maintenance Station Server / WinCC Server Windows Server 2003 SP1
Maintenance Station Client / WinCC Client Windows XP Professional SP2 / Windows Server 2003 SP1


Hardware Requirements
System Clock rate Main memory Hard disk space required
Engineering Station 2.8 GHz 1 GB 15 GB
Maintenance Station Stand-alone / WinCC Station "Single-user" 2.8 GHz 1 GB 15 GB
Maintenance Station Server / WinCC Server 2.8 GHz 1 GB 15 GB
Maintenance Station Client / WinCC Client 2.8 GHz 512 MB 15 GB

For further hardware requirements, please refer to the product documentation.


Ordering Information SIMATIC Maintenance Station 2007 SP1
Part no. Description
6ES7 840-0WD00-0YA0 SIMATIC Maintenance Station 2007 Engineering SW (Floating License) RT license for 100 devices (Single License, count relevant)
6ES7 840-0WD10-0YD0 SIMATIC Maintenance Station Powerpack 100 RT license for 100 additional devices (Single License, count relevant)
6ES7 840-0WD20-0YD0 SIMATIC Maintenance Station Powerpack 500 RT license for 500 additional devices (Single License, count relevant)
6ES7 840-0WD30-0YD0 SIMATIC Maintenance Station Powerpack 1000 RT license for 1000 additional devices (Single License, count relevant)

Related Links


Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive
Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com

Contact Siemens Australia & New Zealand

Siemens Australia

885 Mountain Hwy
Bayswater VIC 3153
Australia
Tel: 137 222
Fax: 1300 360 222
Email: customercare.au@siemens.com

Siemens New Zealand

55 Hugo Johnston Drive
Penrose, Auckland
New Zealand
Tel: +64 (9) 580 5500
Fax: +64 (9) 580 5501
Email: customercare.nz@siemens.com
|

Solution Areas

Solutions - Go